Understanding the principle and benefits of the different ultrasonic flow measurement methods: Transit time differential, Doppler and cross-correlation
ArticleMeerdere industrieën03.12.2024
In het kort
Transit time differential method: Measures flow by comparing the time it takes for ultrasonic pulses to travel with and against the fluid flow. The difference in transit times is proportional to the flow velocity.
Doppler method: Uses the Doppler effect to measure flow by detecting frequency shifts in sound waves reflected off particles or bubbles in the fluid.
Cross-correlation method: Measures flow by tracking the time it takes for disturbances or patterns in the flow to travel between two points. This method is effective for high flow velocities and fluids with entrained particles or gas bubbles.
InhoudsopgaveInhoudsopgave
Transit time differential method (time-of-flight)
This method is used for measuring liquids and gases and utilizes the fact that the propagation velocity of sound waves within a fluid is directly influenced by the velocity of that fluid. Expressed in simple terms, swimming against the flow requires more power and time than swimming with the flow. Ultrasonic flow measurement utilizing the transit time effect is based on this simple physical fact (see Fig. 1).
In this method, the sensors work in pairs. One pair of sensors or more are mounted on the pipe, and they emit and receive ultrasonic pulses in sequence (denoted by signal t1 and t2 in the below figure). At “zero flow”, signal t1 is similar to t2, i.e. without transit time delay. But with a flowing fluid, the ultrasonic waves require differing lengths of time (flow dependent) to reach the other sensor. This results in a transit time (t2 – t1). If the distance between the two sensors is known, then the measured transit time difference is directly proportional to the flow velocity. Both sensors are connected to a transmitter. The transmitter excites the sensors to generate sound waves and measures the transit time of these waves propagating from one sensor to the other:
Fig. 1: Ultrasonic flow measurement using the transit time differential method. The speed at which sound waves propagate varies depending on the fluid velocity and its direction.
Doppler method for flowmeters
A Doppler flowmeter uses the Doppler effect (sometimes referred to as the Doppler shift) to measure flow. This phenomenon of physics is familiar to all of us in our everyday lives. It involves the reflection of waves from moving objects. The audio frequency of an ambulance siren, for example, falls distinctly once it has passed. Thus, a Doppler shift is an increase (or decrease) in the frequency of sound waves as the distance between audio source and receptor increases or decreases.
Doppler meters work only if the fluid contains particles, gas bubbles or similar, which will reflect the injected sound waves. A Doppler meter requires one sensor which acts as both transmitter and receiver. (Fig. 2).
Fig. 2: Ultrasonic flow measurement using the Doppler effect. The frequencies of emitted (f1) and reflected (f2) ultrasound waves vary depending on flow velocity of the transported particles/bubbles.
Cross-correlation method
Next to the doppler and transit time differential method, flow can also be measured with the help of a cross-correlation method. This method measures flow by sensing the passage of disturbance or flow profile pattern in the flow at one measuring point and detects how much time (transit time) that disturbance needs to travel to the next measuring point. The distance of the two measuring points (Δx) is known, and the travel time is measured. Based on that, the flow velocity and the volume flow can be calculated.
This method can be used for measurements with very high flow velocities and/or high contents of entrained gas bubbles or particles. It needs a powerful signal processing and hardware to process the many needed calculations and comparisons of disturbances and/or patterns.
We offer a complete portfolio for versatile and economical flow measurement of gases and liquids up to a nominal diameter DN 4000. Click here to see all ultrasonic flowmeters.
Op 03 juni brengt Lab Technology onderzoekers en professionals die in en rond het lab werken samen om sneller, flexibeler en veiliger te werken; samen op weg naar Lab Technology 2.0
Wilt u deelnemen aan een van onze evenementen? Selecteer op categorie of op industrie.
Wij letten op uw privacy
We maken gebruik van cookies om uw browse-ervaring te verbeteren, statistische gegevens te verzamelen om de site-functionaliteit te optimaliseren en om reclame of content op maat te presenteren.
Door "Accepteer alles" te selecteren gaat u akkoord met ons gebruik van cookies.
Bekijk voor meer details onze cookie-richtlijnen .