Title

Zoek op trefwoord, order- of productcode of serienummer, bv. “CM442” of “Technische informatie”
Voer tenminste 2 karakters in om het zoeken te starten.
  • Geschiedenis

From the laboratory to the field with Raman spectroscopy

Evonik's scalable PAT solution – for greater efficiency, safety, and quality in specialty chemicals manufacturing

Industrie: Chemie
Process Engineer and Endress+Hauser Raman probe at Evonik

Samenvatting

In partnership with Endress+Hauser, Evonik has successfully integrated Raman spectroscopy as a powerful process analysis technology (PAT) from the laboratory to pilot plants, right through to production. This technology delivers real-time data, increases efficiency, reduces costs, and improves product quality. Its flexibility, scalability, and safety make it the key to new savings potential in chemical process development. Customers can benefit directly from this acquired expertise to optimize their own development and production processes in a sustainable manner.

The results: Greater efficiency, safety, and quality

16

installed Raman Rxn2 analyzers

50+

measuring points with Raman Rxn probes

Raman spectroscopy from Endress+Hauser has established itself as a key PAT tool at Evonik. It enables significant efficiency gains, cost reductions, and faster market launch of new products.

Results include:

  • End-to-end process analysis from the laboratory to production
  • Real-time measurements possible at several measuring points at the same time
  • Inline measurements replace manual sampling
  • Suitability for pilot plants with low volumes
  • Reliable operation even under difficult conditions (e.g., ATEX zones)
  • Reduction in the time to market
  • Cost reduction through elimination of laboratory evaluations and reduced personnel costs
  • Increased safety
  • Internal acceptance and acquisition of expertise
Photo of Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG

"With Raman spectra, you might be able to assign isolated peaks to individual substances in the mixture. This significantly reduces the calibration effort and quickly leads to quantitative results."

Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG

The challenge: Find a versatile, real-time lab-to-process solution

Back in 2016, Evonik launched its company-wide “lab to process” strategy with the aim of embedding PAT technologies early on in process development. Evonik was looking for a process analysis technology that would efficiently support the entire development and optimization process while also helping to reduce costs. The goal was to find a solution that not only provides accurate real-time data but is also versatile enough to be used in a wide variety of process environments – from the laboratory to production.

The technology should:

  • be universally applicable for a wide range of chemicals, states of matter and process conditions
  • be flexible and scalable from the R&D lab to large-scale production facilities
  • be quick to integrate in order to shorten development times and reduce time to market
  • improve product quality through continuous inline measurements
  • function reliably even under demanding conditions such as ATEX zones

Our solution: A scalable PAT Endress+Hauser Raman spectroscopy system

Endress+Hauser provided Evonik with a customized solution based on Raman spectroscopy – a technology that meets all of the requirements outlined. The systems are characterized by their exceptional modularity and versatility. Thanks to optical fibers and various probe types, they can be easily integrated into a wide variety of installation situations. Up to four independent channels enable simultaneous monitoring of multiple measuring points – a clear advantage for complex processes.

The chemometric suitability of the spectra offers particular added value – due to compatibility with all common chemometric programs, these can be analyzed directly on the spectrometer in a way that is versatile, intuitive, and achieved in real time. This allows qualitative and quantitative data to be recorded and interpreted immediately during the process – without any time-consuming manual sampling.

Raman spectroscopy was successfully used for the first time in a pilot plant for the development of hydrogenation processes. The probe was integrated into a 6 mm pipe – significantly smaller than in production facilities. Instead of daily NMR sampling, the technology now enables inline measurements to be taken every single minute, and the process continuously monitored.

This process is efficient, precise, and safe. In pilot plants with low volumes in particular, the system composition remains unchanged because no samples need to be taken. This not only saves time and money but also increases safety for both personnel and plant.

Hazardous area use

Thanks to its standardized and certified components, the Raman system can even be used in ATEX zones at a cost that is reasonable. For use in potentially explosive atmospheres, Evonik also uses the Liquiphant Vibronic level switch. This ensures that no flammable gas mixture can form in the laser beam of the Raman probe – a decisive contribution to process safety.

Testimonial

Photo of Dr. Roland Peschke, PAT expert at specialty chemical manufacturer Evonik

“The requirements for PAT measurement systems are particularly high, especially in the harsh environment of process plants and the need to comply with ATEX regulations. Raman spectroscopy has established itself as a robust and reliable tool in this area.” - Dr. Roland Peschke, PAT expert at Evonik Oxeno

Global roll out

This system has enabled Evonik not only to increase efficiency and quality in process development, but also to successfully transfer technology from the laboratory to production – a real key to new savings potential. Following successful implementation in Germany, Raman technology is now being rolled out internationally in Evonik’s first production plants – supported by the global expertise of Endress+Hauser.

Free download

Download the case study

Want access to the full case study as a PDF? Download a copy to read at your convenience, save for future reference, or share with colleagues.

Download the case study

Neem contact met ons op

Heb u interesse in onze producten? Wilt u ons meer vertellen over uw toepassing?

Laat ons alstublieft zo gedetailleerd mogelijk weten hoe we u kunnen helpen. Op die manier kunnen we u met het best mogelijke antwoord benaderen.

Products and services used

/

Related solutions and technology

Optische analyse

Optische analysesystemen voor het monitoren van de samenstelling en concentratie in vaste stoffen, vloeistoffen, slurries, deeltjes en gassen – voor laboratorium-, proces- en emissiemonitoring.

Meer informatie

Bewaking van effluentlozing 

Beheer de afvalwaterlozing binnen de wettelijke grenzen met een volledige, betrouwbare bewaking van continue waarden en een snelle reactie op verontreiniging.

Lees meer

Waterstofmeting in pijpleidingen voor aardgas

Snelle, continue waterstofmeting in pijpleidingen voor aardgas maakt een veilige bijmenging, kwaliteitsborging en dynamische beheersing mogelijk met behulp van Raman-spectroscopie - zonder verbruiksartikelen of affakkelen

Lees meer

Kwaliteitsanalyse van biomethaan voor een veilige gasinjectie conform de regelgeving 

Zorg voor een betrouwbare biomethaankwaliteit met snelle, nauwkeurige onlinemetingen van H₂S, waterdauwpunt en kritieke parameters voor een veilige teruglevering aan het net en een efficiënt proces. 

Lees meer

Membranen voor omgekeerde osmose beschermen met onlinebewaking van de waterkwaliteit voor ontzilting 

Betrouwbare online waterkwaliteitsbewaking ter bescherming van RO-membranen (Reverse Osmosis; omgekeerde osmose) vermindert de reinigingsinspanning en verlengt de levensduur van membranen in toepassingen voor ontzilting en waterhergebruik

Lees meer

Detectie van lekkages in cryogene tanks (LNG, ethyleen, LPG en ammoniak)

Detecteer cryogene tanklekkages vroegtijdig en blijf de situatie de baas. Endress+Hauser levert continue, uiterst betrouwbare temperatuurbewaking om mensen, assets en belangrijke infrastructuur te beschermen.

Lees meer

Realtime CCUS-meting & -verificatie

Ontsluit de toekomst van koolstofafvang: nauwkeurig, betrouwbaar en aangepast voor compacte fase-toepassingen

Lees meer

Oplossingen voor continue emissiebewaking voor het waarborgen van compliantie

Oplossingen voor continue emissiebewaking voor het waarborgen van compliantie

Meer informatie

FAQs

Company logo of: Evonik Industries AG

Evonik Industries AG, met hoofdzetel in het Duitse Essen, is een wereldleider op het gebied van speciale chemicaliën. Dankzij de passie voor innovatie en technische uitmuntendheid gaat het bedrijf verder dan traditionele chemie voor het creëren van duurzame oplossingen voor industrie en maatschappij. Evonik heeft productiefaciliteiten in 27 landen op zes continenten.